FRDM-KL25Z on board sample code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z on board sample code

Jump to solution
6,533 Views
hotashu
Contributor III

I recenetly got a FRDM-KL25Z board,  i want to find the on board demo souce code . i see there is one KL25_SC.exe , but which project inside is for the out of factory FRDM-KL25Z board?

0 Kudos
Reply
1 Solution
3,146 Views
Mario_Guardado
Senior Contributor I

Hello Hotas,

You can find the sample code for FRDM-KL25 in the KL25_SC.exe file.

The following path is related to the Freedom Demo source code.

kl25_sc_rev6\klxx-sc-baremetal\src\projects\FRDM_KL25ZDemo

The following path is related to the Freedom Demo project (IAR).

kl25_sc_rev6\klxx-sc-baremetal\build\iar\FRDM_KL25ZDemo

Regards,

Mario

View solution in original post

0 Kudos
Reply
3 Replies
3,146 Views
TomasVaverka
NXP TechSupport
NXP TechSupport


Hotas,

The FRDM-KL25Z board comes out of the box preprogrammed with the FRDM_KL25Z_OOBE_Demo.srec example. This demo cycles through several colors on the RGB LED, changes the color mix of the RGB LED based on the accelerometer data and uses the capacitive slider to change the brightness of the LED.

The FRDM_KL25Z_OOBE_Demo.srec file as well as other examples is stored in the Precompiled Examples folder of the attached FRDM-KL25Z Quick Start Package.

Check out this video presentation or have a look at the FRDM-KL25Z Quick Start Guide for more information.

Regards,

Tomas

0 Kudos
Reply
3,146 Views
hotashu
Contributor III

hello Tomas,

thank you for your answer?

i knew FRDM-KL25Z_QSP.zip , but there is no project and source code inside. does freescale provide source code of it?

why freescale only like to provide preprogrammed file but no source project?

I appreciate your help

0 Kudos
Reply
3,146 Views
Mario_Guardado
Senior Contributor I

Hello Hotas,

You can find the sample code for FRDM-KL25 in the KL25_SC.exe file.

The following path is related to the Freedom Demo source code.

kl25_sc_rev6\klxx-sc-baremetal\src\projects\FRDM_KL25ZDemo

The following path is related to the Freedom Demo project (IAR).

kl25_sc_rev6\klxx-sc-baremetal\build\iar\FRDM_KL25ZDemo

Regards,

Mario

0 Kudos
Reply