FRDM-KL25Z Rev. F Schematics? Or Differences vs. Rev. E?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL25Z Rev. F Schematics? Or Differences vs. Rev. E?

6,531件の閲覧回数
alexdean
Contributor III

Hi, does anyone have the schematics for Revision F of the FRDM-KL25Z PCB?  The latest schematics I see online are for Revision E. Or, what changes are there from the E revision?

Thanks,

Alex

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

5,841件の閲覧回数
MacD1
Contributor I

original post was @June 2015, and still I could not find rev F schematic,

0 件の賞賛
返信

5,833件の閲覧回数
MacD1
Contributor I

I got this.

Changing C12
from 1uF to 0.1uF
to fix yield issue

 

thanks

 

0 件の賞賛
返信

6,090件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Alex,

the only official available FRDM-KL25Z schematic is Rev E.  I don't have any information for Rev F.

here is the Revisions & Change Log from Rev D to Rev E.

pastedImage_1.png

more information can be check from the first page of Freedom Kl25 Rev E schematic

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL25Z_SCH_REV_E.pdf

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,558件の閲覧回数
723679104
Contributor I

HI,

I had a borad for REV F , Can you send PCB REV F to me ?

thanks

 

br

sam

0 件の賞賛
返信

6,090件の閲覧回数
alexdean
Contributor III

Thanks, Zhang Jun. Maybe someone else knows?

In any case, I compared the boards and didn't see any obvious differences, so perhaps it's a minor change.

Regards,

Alex

0 件の賞賛
返信