FRDM-KL25Z: Device could not be powered up.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL25Z: Device could not be powered up.

2,496件の閲覧回数
johntt
Contributor II

Hi,

I'm trying to debug/program FRDM-KL25Z with Keil uVision without success. I have message:

AGDI - Cortex-M Error: Device could not be powered up.

More detailed information about this error:

Debug block on the device could not be powered. Debug block on the target is not working properly. Mainly caused by target problems: debug block not powered and clocked properly

Device works with last application programmed but I can not program it any more.

This error has appeared after I debugged application with RTC/LPTMR with direct register modification. Could it be the main reason or something else?

Is that means chip is broken?

0 件の賞賛
返信
1 返信

1,885件の閲覧回数
johntt
Contributor II

I tried to place resistor of 1M in R25 and in programmer settings I only chose 'Erase Full Chip'. Erasing succeeded. Then I took out resistor and tried to debug /program and it seems to work.

0 件の賞賛
返信