FRDM-KL25Z BOOTLOADER update?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z BOOTLOADER update?

Jump to solution
4,105 Views
raymetz100
Contributor II

When I hold in RESET, connect to my laptop USB, and release RESET, I get a BOOTLOADER drive in Ubuntu Linux 14.10.  I open the SDA_INFO.HTM and get this...

Board Name is: FRDM-KL25Z

MicroBoot Kernel Version is: 1.05

Bootloader Version is: 1.09     (I believe I want this to say 1.11)

Application Version is: 0.00  (I believe I want this to say

PEMicro FRDM-KL25Z Mass Storage/Debug App

Application Version is: 1.14  ??)

DUID is: 15833938-AE6C81CB-3780E805-BA9BE678

EUID is: 1D21A239-410E8741-18800A22-A0A468D6

TUID is: 74823938-473281CF-375C981C-B85CE678

TOA is: 86B6E505-DD85231C-41E6B687-89728A14

TOA2 is: 86B6E505-CE21DE8B-CDE430D7-CA7FFCD5

SUID is: 86B6E505-6C47A61D-37239804-8003EC65

Stickers on my board say:

700-27556 rev A

SCH-27556 rev F

serial number EB14400292

How do I know if this is the latest or not?

I downloaded Pemicro_OpenSDA_Debug_MSD_Update_Apps_2015_03_12.zip from http://www.pemicro.com/opensda/, unzipped, and see these:

DEBUG-APP_Pemicro_v108.SDA

DEBUG_OpenSDA_for_MBED_Bootloader_by_Pemicro_v108.bin

BOOTUPDATEAPP_Pemicro_v111.SDA

MSD-DEBUG-FRDM-KL25Z_Pemicro_v114.SDA

What's the difference between these files?  Do I need to install them in any order or all at once?  I tried copying each of the three .SDA and .BIN files to my BOOTLOADER drive and restarting my FRDM board, but they just disappear and I don't see any version numbers changing in SDA_INFO.HTM.  Do I already have the latest version?  I see 108, 111, and ,114 on the files, but only 105 and 109 on my SDA_INFO.HTM so I don't think it installed.

Also, when I first plugged in my FRDM-KL25Z, it slowly blinked though 8 colors then the accelerometer fade mode.  Now when I plug it in without holding RESET, it just sits black with no LEDs.  I'm not sure if I ruined the software somehow.  It also used to appear as a FRDM-KL25Z drive with these files:

SERCDC89.INF

SERCDC89.CAT

LASTSTAT.TXT

SDA_INFO.HTM

FSL_WEB.HTM

TOOLS.HTM

Now, I don't get anything.unless I do the RESET BOOTLOADER mode.  Did I brick my board?  Good thing they are only $13.  I have two more on the way.

Thanks,

Ray Metz

0 Kudos
Reply
1 Solution
3,048 Views
raymetz100
Contributor II

Thanks Erich. I read your link and got some great ideas.

I tried from Linux first and still no luck.

Then I went back to Windows 8.1 and installed this fix:

How do I prevent system volume information files from showing up in my - Microsoft Community

Then it still didn't work, but I tried using Windows CMD dos window to copy the files instead of drag and drop windows explorer and it worked first try.

My versions are this now:

Board Name is: FRDM-KL25Z

MicroBoot Kernel Version is: 1.05

Bootloader Version is: 1.11

Installed Application: PEMicro FRDM-KL25Z Mass Storage/Debug App

Application Version is: 1.14

Ray

View solution in original post

0 Kudos
Reply
2 Replies
3,048 Views
BlackNight
NXP Employee
NXP Employee

Hi Ray,

it seems you probably did not perform the steps in the correct order. You might have a look here:

http://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-free...

(Screenshots for Windows, but same applies to Linux).

Erich

3,049 Views
raymetz100
Contributor II

Thanks Erich. I read your link and got some great ideas.

I tried from Linux first and still no luck.

Then I went back to Windows 8.1 and installed this fix:

How do I prevent system volume information files from showing up in my - Microsoft Community

Then it still didn't work, but I tried using Windows CMD dos window to copy the files instead of drag and drop windows explorer and it worked first try.

My versions are this now:

Board Name is: FRDM-KL25Z

MicroBoot Kernel Version is: 1.05

Bootloader Version is: 1.11

Installed Application: PEMicro FRDM-KL25Z Mass Storage/Debug App

Application Version is: 1.14

Ray

0 Kudos
Reply