FRDM-KL03Z serial problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KL03Z serial problem

1,396 次查看
ballen
Contributor I

Just started with a FRDM-KL03Z development board and have a very basic problem. I'm using TeraTerm, all serial port params are correct, but all I get on the terminal screen is endless "alpha" characters, not the "x=; y=" display shown in the on-line introduction to the FRDM board. The LED tilt program appears to be working correctly. Any suggestions?

Thanks,

Bill

0 项奖励
回复
2 回复数

1,299 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bill,

Please download the SDK_2.2_FRDM-KL03Z and then test the bubble example.

Select FRDM-KL03Z.png

download SDK_2.2_FRDM-KL03Z.png

bubble.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,299 次查看
mjbcswitzerland
Specialist V

Bill

Try loading references from here:
http://www.utasker.com/kinetis/FRDM-KL03Z.html

Regards

Mark

Open Source uTasker project for better KL03 performance at
http://www.utasker.com/forum/index.php?topic=1721.msg7086#msg7086
including compatibility with 10 IDEs and KL03 simulation (no portability issues since the same code runs on almost all Kinetis parts)

0 项奖励
回复