FRDM-KL03Z serial problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL03Z serial problem

1,403件の閲覧回数
ballen
Contributor I

Just started with a FRDM-KL03Z development board and have a very basic problem. I'm using TeraTerm, all serial port params are correct, but all I get on the terminal screen is endless "alpha" characters, not the "x=; y=" display shown in the on-line introduction to the FRDM board. The LED tilt program appears to be working correctly. Any suggestions?

Thanks,

Bill

0 件の賞賛
返信
2 返答(返信)

1,306件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bill,

Please download the SDK_2.2_FRDM-KL03Z and then test the bubble example.

Select FRDM-KL03Z.png

download SDK_2.2_FRDM-KL03Z.png

bubble.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,306件の閲覧回数
mjbcswitzerland
Specialist V

Bill

Try loading references from here:
http://www.utasker.com/kinetis/FRDM-KL03Z.html

Regards

Mark

Open Source uTasker project for better KL03 performance at
http://www.utasker.com/forum/index.php?topic=1721.msg7086#msg7086
including compatibility with 10 IDEs and KL03 simulation (no portability issues since the same code runs on almost all Kinetis parts)

0 件の賞賛
返信