FRDM-KL03Z - VREF and UART0_RX (Bootloader)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KL03Z - VREF and UART0_RX (Bootloader)

1,637 次查看
aes_mike
Contributor III

This is a two part question:

1. How or where in the documentation does the internal VREF get routed over to the ADC or is this intended to drive a sensor only?

I was hoping to use the VREF as a voltage reference to the ADC, but not clear to me that it is possible.

2. If VREF can be used by the ADC, then how does one deal with UART0_RX at PTB2?  Can it be re-routed somehow?  But from what I understand the bootloader will try to use UART0 with TX/RX at PTB1 and PTB2, respectively.

Can someone explain this?

标记 (4)
0 项奖励
回复
1 回复

1,451 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

1. How or where in the documentation does the internal VREF get routed over to the ADC or is this intended to drive a sensor only?

I'd like to suggest that you can find detailed information of the VREF_OUT implement in the Chapter 30: Voltage Reference (VREF) in the KL03's reference manual.

And you can download it through it link as below.

http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&WT_TYPE=Reference%2...

2. If VREF can be used by the ADC, then how does one deal with UART0_RX at PTB2?  Can it be re-routed somehow?  But from what I understand the bootloader will try to use UART0 with TX/RX at PTB1 and PTB2, respectively.

It's not available to use the VREF_OUT and UART0_RX at the same time, you can only choose one specific function of the pin.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复