FRDM-KEAZ128 demo source code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KEAZ128 demo source code

3,266 次查看
parkmanchan
Contributor I

Hi,

   Is the source code for the demo that comes with the FRDM-KEAZ128 available somewhere? It would be great if I can restore the board after experimenting.

  Thanks.

Park

标记 (1)
0 项奖励
回复
3 回复数

2,760 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Park man Chan,

Please download the FRDM-KEA Quick start package from FRDM-KEAZ128 page.

FRDM-KEA Quick start package.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,760 次查看
parkmanchan
Contributor I

Hi Robin,

   Are you referring source in Code Project Examples for FRDM-KEAZ128.zip in Quick Start Package v8/Code Project Examples and Sample Drivers (Evaluation Grade Only)/FRDM-KEAZ128/Code Project Examples for FRDM-KEAZ128?

   After checking sources in Lab1 - Lab11, I haven't found source with the same behavior as the out-of-box demo, in which two different demos in controlling the LED are selected by pressing switches. Am I looking at the right place?

Thanks

0 项奖励
回复

2,760 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I did not find the Out-of-Box Demo project for FRDM-KEAZ128.
But the Lab6_Blinky_FTM_ADC_KEA128 is very similar to Example #1

Out-of-Box Demo 1.png

Best Regards,

Robin

0 项奖励
回复