FRDM KE04Z won't exit bootloader mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM KE04Z won't exit bootloader mode

1,565 Views
andrewwenger
Contributor I

Hi I am really new with FRDM boards and am working in a group for a university project. I am following the quick start guide for the FRDM KE04Z and am in the open SDA bootloader mode. I have followed the instructions but when I disconnect the board and plug it back in it still comes up as bootloader drive vs the FRDM drive. Can anyone tell me how to fix this?

0 Kudos
Reply
1 Reply

1,383 Views
mjbcswitzerland
Specialist V

Andrew

If the board shows up as bootloader it means that either the RESET switch is being held down on power up or there is no code valid loaded.

If you loaded debugger code to it check the "status" file which will indicate whether the loading was sucessful or not (immediately after loading). If it failed or an invalid file was loaded it will stay in the bootloader mode.

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker Kinetis support  / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply