Hi All
FRDM-KE02 trouble, always in debugging mode without reset button pressed, LED always blinks.
I worked with FRDM-KE02Z via CodeWarrior. I just tried Flash File to target. And got the same trouble with two board
Windows 7
CodeWarrior: 10.6. Build Id:140329
FRDM-KE02Z firmware updated
Board Name is: FRDM-KE02Z
MicroBoot Kernel Version is: 1.05
Bootloader Version is: 1.11
Installed Application: PEMicro FRDM-KE02Z Mass Storage/Debug App
Application Version is: 1.14