FRDM-K82F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K82F

5,016 Views
kentachang_melt
Contributor II

Hello,

I buy the FRDM-K82F, I want to find the schematic of FRDM-K82F.

Please let me know where to find the FRDM-K82F schematic ?

Regards,

Kenta

0 Kudos
Reply
3 Replies

4,735 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Kenta,

You can go to downloads page of FRDM-K82F: NXP Freedom Development Platform for Kinetis K82, K81, and K80 MCUs and download the FRDM-K82F - Printed Circuit Board bill of materials and design files.

The schematic can be found in that folder named "spf-28748_b2.pdf".

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,730 Views
kentachang_melt
Contributor II

Hello Robin,

Thank you so much.

The schematic "spf-28748_b2.pdf" is found.

Best Regards,

Kenta

0 Kudos
Reply

4,729 Views
mjbcswitzerland
Specialist V

Hi

Go to

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus:KIN...

and do a search for FRDM-K82F and the first link is http://cache.nxp.com/files/32bit/hardware_tools/schematics/FRDM-K82F-SCH.pdf?fsrch=1&sr=1&pageNum=1

This leads to "Page not found"

Instead search just for FRDM-K82F and then it will lead you to the board's page: http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/ides-for...

The trick with the evaluation boards is that the diagrams are generally not found under documentation but instead under downloads. However the same download link leads also to a "Page not found".

Therefore the web site has a problem at the moment - in the meantime I am attaching the FRDM-K82F Rev. B2 circuit diagram as PDF which can be downloaded until the missing file is fixed.

Regards

Mark

See also http://www.utasker.com/kinetis/FRDM-K82F.html

0 Kudos
Reply