FRDM-K82F - boot loader available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K82F - boot loader available

1,457件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

For users of the new FRDM-K82F board I would like to point out that serial loaders have been prepared which allow:

- USB compatible KBOOT

- KBOOT compatible UART

- UART developer's loader

- USB-MSD device

- UART SREC

- USB-MSD-Host Memory Stick

Projects requiring one or more of these modes (also multiple at the same time if desired) thus can avoid porting efforts since they are ready for CW, KDS, IAR, Keil, Atollic, Green Hills, Crossworks or CooCox builds.

The most popular (USB-MSD and KBOOT composite) can be downloaded from the following link, and there is an interesting application that can be tried that allows the FRDM-K82F to act as a virtual network adapter (RNDIS) to the host so that it can run a web server, FTP server, Telnet etc. for the connected PC: http://www.utasker.com/kinetis/FRDM-K82F.html

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K80: http://www.utasker.com/kinetis/FRDM-K82F.html / http://www.utasker.com/kinetis/TWR-K80F150M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信
0 返答(返信)