FRDM-K82 Bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K82 Bootloader

1,598 次查看
sanket_joshi
Contributor I

HI,

I am using FRDM-K82 board which has open SDA on board. I am unable to enter bootloader mode. I tried pressing the reset button and then powering it up. Still it is not working.

标记 (1)
0 项奖励
回复
1 回复

1,462 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

It has been reported that OpenSDA v2/2.1 bootloader could be corrupted when the board is plugged int...

bootloader and firmware application.png

Please check if the your board is in bricked state.

bricked state.png
If so please refer DAPLink bootloader updates with external debug probe to recover the bootloader.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复