FRDM-K82 Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K82 Bootloader

1,668件の閲覧回数
sanket_joshi
Contributor I

HI,

I am using FRDM-K82 board which has open SDA on board. I am unable to enter bootloader mode. I tried pressing the reset button and then powering it up. Still it is not working.

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,532件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

It has been reported that OpenSDA v2/2.1 bootloader could be corrupted when the board is plugged int...

bootloader and firmware application.png

Please check if the your board is in bricked state.

bricked state.png
If so please refer DAPLink bootloader updates with external debug probe to recover the bootloader.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信