FRDM-K66F OpenSDA interface only starts up in Bootloader mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K66F OpenSDA interface only starts up in Bootloader mode

1,366 Views
mrice
Contributor I

As described, my FRDM-K66F OpenSDA interface only ever starts in bootloader mode, despite the fact that I am not holding down the reset button while plugging it in.  Yesterday it was working fine and I was able to debug code through the interface from MCUXpresso.  

The green LED DS2 is blinking a couple times a second and the device appears as a drive in Explorer (Windows 10).  

This is our second FRDM-K66F; the first one doesn't work now because we tried to upgrade the OpenSDA firmware and the device bricked.  A second board was brought in while we wait for a J-link to manually fix the first board.  

Any help would be appreciated.

 

 

0 Kudos
Reply
1 Reply

1,355 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi mrice,

Old FRDM-K66F use openSDA v2/2.1.  It could be corrupted when the board is plugged into a Windows 10 machine. You have to upgrade to v2.2.

https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem...

Here is some thing useful

Bricking and Recovering OpenSDA Boards in Windows 8 and 10 | MCU on Eclipse

DAPLink bootloader update | Mbed

Recovering OpenSDA Boards with Windows 10 | MCU on Eclipse

 

Regards,

Jing

0 Kudos
Reply