FRDM K66 - USB Host MSD Fatfs FreeRTOS Example Problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM K66 - USB Host MSD Fatfs FreeRTOS Example Problems

2,167 次查看
ReySinTrono
Contributor I

Hello,

I'm testing example project usb host msd fatfs with FreeRTOS in FRDM K66 with "MSD_FATFS_THROUGHPUT_TEST_ENABLE (1U)".
The problem is that the test fails with several FAT32 USB Flash Drives. For example:

1. TOSHIBA TransMemory USB 2.0   [7759,46 MB]    (15155200 512-byte sectors):  Test Write Ok, Test Read Fail.

2. Lexar USB Flash Drive  USB 2.0   [16 GB]    (31258624 512-byte sectors): Test Write Error, Test Read Not Executed.

3. Kingston DataTraveler USB 3.0   [7751,07 MB]    (15138816 512-byte sectors): Test Write Ok, Test Read Ok.

4. Generic Flash Disk USB 2.0 [7780,43 MB] (15196160 512-byte sectors): Test Write Ok, Test Read Error. 

Any ideas?

Regards.

0 项奖励
回复
2 回复数

1,846 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Juande:

Please see the below table for the list of USB devices tested with the USB Host stack. You also can get it from the release note.

pastedImage_1.png

pastedImage_2.png

Thank you for your feedback, I will send your issue to the develop team.

Regards

Daniel

0 项奖励
回复

1,846 次查看
ReySinTrono
Contributor I

Something new?

Thanks.

0 项奖励
回复