FRDM K64f failing launch sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM K64f failing launch sequence

2,130 Views
smith1
Contributor II

I have two FRDM K64f boards, and I am trying to get CAN communication to work between them, and now one of my boards when I try to program it says that there is a failure in launch sequence. In order to program both boards, I was unplugging one of the boards, so I could program the other, which I think may have to led to this, but I'm not sure how to fix this issue.

Also, if you know how I could program both boards without unplugging one of them that would be helpful as well.

Tags (2)
0 Kudos
Reply
3 Replies

2,047 Views
BlackNight
NXP Employee
NXP Employee

Hi Timothy,

you have to specify different port numbers for each connection, see Debug Multiple Boards with GDB at the Same Time | MCU on Eclipse . Then you can debug multiple boards the same time.

I hope this helps,

Erich

0 Kudos
Reply

2,047 Views
smith1
Contributor II

I've fixed my issue by resetting the firmware on the board, but are there any suggestions on programming one of boards without unplugging the other?

0 Kudos
Reply

2,047 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Timothy Smith,

     You can try the Segger JLINK's method: multiple devices in the scan chain.

   More details, please refer to this document:

https://www.segger.com/admin/uploads/productDocs/UM08001_JLink.pdf 

Page 180, chapter 5.3 JTAG interface.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply