FRDM-K64F "blocked" and I can't program it anymore.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM-K64F "blocked" and I can't program it anymore.

跳至解决方案
1,139 次查看
is709667
Contributor I

Hello, good day.

I was doing some test with a simple code to turn the LEDs on in a certain color sequence (I had tested the code before and it worked fine). But, suddenly the K&4disconnected  and it kind of "blocked" itself, now I am unable to load any code into the K64. I get the following error:

Error 1.jfif

I tried to check the K64 with J-Link Commander and also I an error, it is the following one:

Error 2.jfif

Also, I noticed that the K64 starts to warm up when I try to load code.

Can you please help with this? I don't really know why this started to happen.

Best regards

0 项奖励
回复
1 解答
1,072 次查看
ErichStyger
Specialist I

>Also, I noticed that the K64 starts to warm up when I try to load code.

That is indicating to me that you have a hardware failure and the K64 is damaged (ESD maybe?).

Is this your custom board or the FRDM-K64F?

I'm affraid that you would have to change/replace the MCU/Board.

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,073 次查看
ErichStyger
Specialist I

>Also, I noticed that the K64 starts to warm up when I try to load code.

That is indicating to me that you have a hardware failure and the K64 is damaged (ESD maybe?).

Is this your custom board or the FRDM-K64F?

I'm affraid that you would have to change/replace the MCU/Board.

I hope this helps,

Erich

0 项奖励
回复
1,072 次查看
is709667
Contributor I

Oh dear, well, thanks a lot for the quick response. Do you know if there is some warranty that I can use? I bought the K64 about 2 months ago.

Regards

0 项奖励
回复