FRDM-K64F as programmer/debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K64F as programmer/debugger

2,504 次查看
joseasensio
Contributor I

Hi everyone.

I have been taking a look at the FRDM-K64F schematic and I have a question.

Can this board be used to program/debug external targets through the openSDA JTAG pin header (J10, page 3)?

Regards.

Jose

0 项奖励
回复
3 回复数

2,220 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复

2,220 次查看
joseasensio
Contributor I

Hi Erich.

In that article the connector used to debug an external target is J9.

So I guess that J10 is used to program/debug the FRDM-K64F on board cpu using a JTAG programmer like Segger J-LINK or similar.

Am I right?

Regards.

Jose

0 项奖励
回复

2,220 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jose,

yes, that's correct. J10 is used to flash/debug the OpenSDA K20 device on the board.

Erich

0 项奖励
回复