FRDM-K64F as programmer/debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64F as programmer/debugger

2,566件の閲覧回数
joseasensio
Contributor I

Hi everyone.

I have been taking a look at the FRDM-K64F schematic and I have a question.

Can this board be used to program/debug external targets through the openSDA JTAG pin header (J10, page 3)?

Regards.

Jose

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,282件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信

2,282件の閲覧回数
joseasensio
Contributor I

Hi Erich.

In that article the connector used to debug an external target is J9.

So I guess that J10 is used to program/debug the FRDM-K64F on board cpu using a JTAG programmer like Segger J-LINK or similar.

Am I right?

Regards.

Jose

0 件の賞賛
返信

2,282件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jose,

yes, that's correct. J10 is used to flash/debug the OpenSDA K20 device on the board.

Erich

0 件の賞賛
返信