FRDM K64F Red&Green light during OpenSDA Debug installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM K64F Red&Green light during OpenSDA Debug installation

2,242件の閲覧回数
kduon013
Contributor I

Hi, currently for my class, I've been closely following our installation instructions for our K64F and Kinetis Design Studio app, but the nearly last step involves installing the 

DEBUG-FRDM-K64F_Pemicro_v108a_for_OpenSDA_v2.0.bin

After pasting that into the  MAINTENANCE, the window will close, and then my board will show a simultaneous red and green light. (This is in Windows 10, which may or may not be part of the problem). That's the main problem.

Obviously something was wrong, but just to make sure, I tried to go ahead and do a sample code in the Kinetis Design Studio. After doing the debug configuration, and clicking debug, it'll run to ~halfway and then ask me to erase:

image.pngimage.pngimage.pngpastedImage_1.png which I'm a little worried might do something weird, so after clicking no to multiple pop-ups:

pastedImage_2.png and then finally:

pastedImage_3.png will pop up.

And so finally at this point, after going through multiple questions and pages, I'm at a standstill. 

I've looked at NXP's website https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...  (but just redirect's me to PEMicro's http://www.pemicro.com/opensda/  page, which already has everything I downloaded.)

I'm not sure if it's ok to try to install the MSB instead of just the DEBUG.bin file, but that's what this website says to do (

https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...  ). 

My bootloader and drivers are all appearing and updated, it's only this debug (.bin) file that I feel so confused about not working. Thanks!

(For even more information I attached the details.txt link that appearing in my MAINTENANCE mode)

image.png

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

2,150件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

When flash is under secure state , it can't program.So when it ask you to erase it to unsecure ,just click yes. it will be ok.

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信