FRDM-K64F Open-SDA failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K64F Open-SDA failure

1,690 Views
MAPC
Senior Contributor I

Hello,

I'm running into a strange situation. Suddenly, I lost FRDM-K64F Open-SDA connection. I followed several posts in this Community, but nothing works. The only thing I didn't try yet was reprogramming K20 with the Open-SDA .srec file, because I don't have a Universal Programmer like U-Multilink or a Segger J-Link.

I don't know what to do anymore.

pastedImage_0.png

pastedImage_1.png

Regards,

Marco Coelho

Labels (1)
2 Replies

1,456 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Marco,

According to your statement, I think the issue mainly form the software of the OpenSDA interface broken.

And it need to reprogram the K20 to fix this issue, so please refer to this thread as follow for details.

OpenSDAv2

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,456 Views
MAPC
Senior Contributor I

Thank you very much, Jeremyzhou!

Thanks to your tips, I could bring my FRDM-K64F back to life and now I can program and debug through MBED GDB OpenOCD Debugger.7

Best regards,

Marco Coelho

0 Kudos
Reply