FRDM K64F Dual SPI interface with AD7606B Not Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM K64F Dual SPI interface with AD7606B Not Working

ソリューションへジャンプ
4,526件の閲覧回数
GRK
Contributor I

Hi,

i am trying  to interface AD7606B ADC IC with FRDM-k64F by Dual SPI interface similar to the Solution 4 in the link Below. 

https://www.analog.com/en/analog-dialogue/raqs/raq-issue-172.html

in my case

SPI0  is  Master ( working properly )

SPI1  is  Slave.  ( Not working )

i want to read AD7606B as fast as possible.

with single SPI it is working But in Dual SPI interface slave is not working.

Attached is the code file

SPI  configuration

スポイラ

/* Master config */
masterConfig.whichCtar = kDSPI_Ctar0;
masterConfig.ctarConfig.baudRate = TRANSFER_BAUDRATE;
masterConfig.ctarConfig.bitsPerFrame = 16U;
masterConfig.ctarConfig.cpol = kDSPI_ClockPolarityActiveHigh;
masterConfig.ctarConfig.cpha = kDSPI_ClockPhaseFirstEdge;
masterConfig.ctarConfig.direction = kDSPI_MsbFirst; //kDSPI_LsbFirst // kDSPI_MsbFirst
masterConfig.ctarConfig.pcsToSckDelayInNanoSec = 1000000000U / TRANSFER_BAUDRATE;
masterConfig.ctarConfig.lastSckToPcsDelayInNanoSec = 1000000000U / TRANSFER_BAUDRATE;
masterConfig.ctarConfig.betweenTransferDelayInNanoSec = 1000000000U / TRANSFER_BAUDRATE;

masterConfig.whichPcs = EXAMPLE_DSPI_MASTER_PCS_FOR_INIT;
masterConfig.pcsActiveHighOrLow = kDSPI_PcsActiveLow;

masterConfig.enableContinuousSCK = false;
masterConfig.enableRxFifoOverWrite = false;
masterConfig.enableModifiedTimingFormat = false;
masterConfig.samplePoint = kDSPI_SckToSin0Clock;

srcClock_Hz = DSPI_MASTER_CLK_FREQ;
DSPI_MasterInit(EXAMPLE_DSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

/* Slave config */
slaveConfig.whichCtar = kDSPI_Ctar0;
slaveConfig.ctarConfig.bitsPerFrame = masterConfig.ctarConfig.bitsPerFrame;
slaveConfig.ctarConfig.cpol = masterConfig.ctarConfig.cpol;
slaveConfig.ctarConfig.cpha = masterConfig.ctarConfig.cpha;
slaveConfig.enableContinuousSCK = masterConfig.enableContinuousSCK;
slaveConfig.enableRxFifoOverWrite = masterConfig.enableRxFifoOverWrite;
slaveConfig.enableModifiedTimingFormat = masterConfig.enableModifiedTimingFormat;
slaveConfig.samplePoint = masterConfig.samplePoint;

DSPI_SlaveInit(EXAMPLE_DSPI_SLAVE_BASEADDR, &slaveConfig);

// DSPI_SlaveTransferCreateHandle(EXAMPLE_DSPI_SLAVE_BASEADDR, &g_s_handle, DSPI_SlaveUserCallback, NULL);
///* Set slave transfer to receive data */
// isTransferCompleted = false;
slaveXfer.txData = NULL;
slaveXfer.rxData = slaveRxData;
slaveXfer.dataSize = TRANSFER_SIZE;
slaveXfer.configFlags = kDSPI_SlaveCtar0;
GPIO_PortSet(GPIOC, 1U << BOARD_RESET_AD_PIN); //PTC3 RESET
//SysTick_DelayTicks(1U); // Delay 1000 ms
for (i = 0; i < 12000; i++)
{__NOP();}
GPIO_PortClear(GPIOC, 1U << BOARD_RESET_AD_PIN); //PTC3 RESET
GPIO_PortSet(GPIOE, 1U << 25U);
/* Start master transfer, receive data from slave */
masterXfer.txData = NULL;
masterXfer.rxData = masterRxData;
masterXfer.dataSize = TRANSFER_SIZE; //kDSPI_MasterPcsContinuous
masterXfer.configFlags = kDSPI_MasterCtar0 | EXAMPLE_DSPI_MASTER_PCS_FOR_TRANSFER | kDSPI_MasterActiveAfterTransfer; //kDSPI_MasterActiveAfterTransfer

slaveXfer.txData = NULL;
slaveXfer.rxData = slaveRxData;
slaveXfer.dataSize = TRANSFER_SIZE;
slaveXfer.configFlags = kDSPI_SlaveCtar0;

assert(NULL != &masterXfer);

uint16_t wordToSend = 0;
uint16_t wordReceived = 0;
uint8_t dummyData = DSPI_GetDummyDataInstance(EXAMPLE_DSPI_MASTER_BASEADDR);
uint8_t bitsPerFrame;
uint32_t command;
uint32_t lastCommand;
uint16_t *txData;
uint16_t *rxData;
uint32_t fifoSize;
uint32_t tmpMCR = 0;
dspi_command_data_config_t commandStruct;

/* If the transfer count is zero, then return immediately.*/
if (&masterXfer.dataSize == 0U)
{
return kStatus_InvalidArgument;
}
DSPI_StopTransfer(EXAMPLE_DSPI_MASTER_BASEADDR);
DSPI_DisableInterrupts(EXAMPLE_DSPI_MASTER_BASEADDR, (uint32_t)kDSPI_AllInterruptEnable);
DSPI_FlushFifo(EXAMPLE_DSPI_MASTER_BASEADDR, true, true);

DSPI_StopTransfer(EXAMPLE_DSPI_SLAVE_BASEADDR);
DSPI_DisableInterrupts(EXAMPLE_DSPI_SLAVE_BASEADDR, (uint32_t)kDSPI_AllInterruptEnable);
DSPI_FlushFifo(EXAMPLE_DSPI_SLAVE_BASEADDR, true, true);

/*Calculate the command and lastCommand*/
commandStruct.whichPcs =
(dspi_which_pcs_t)(1U << ((masterXfer.configFlags & DSPI_MASTER_PCS_MASK) >> DSPI_MASTER_PCS_SHIFT));
commandStruct.isEndOfQueue = false;
commandStruct.clearTransferCount = false;
commandStruct.whichCtar =
(dspi_ctar_selection_t)((masterXfer.configFlags & DSPI_MASTER_CTAR_MASK) >> DSPI_MASTER_CTAR_SHIFT);
commandStruct.isPcsContinuous =
(0U != (masterXfer.configFlags & (uint32_t)kDSPI_MasterPcsContinuous)) ? true : false;

command = DSPI_MasterGetFormattedCommand(&(commandStruct));
commandStruct.isEndOfQueue = true;
commandStruct.isPcsContinuous =
(0U != (masterXfer.configFlags & (uint32_t)kDSPI_MasterActiveAfterTransfer)) ? true : false;
lastCommand = DSPI_MasterGetFormattedCommand(&(commandStruct));

DSPI_SetFifoEnable(EXAMPLE_DSPI_MASTER_BASEADDR,false,false);
DSPI_SetFifoEnable(EXAMPLE_DSPI_SLAVE_BASEADDR,false,false);
/*Calculate the bitsPerFrame*/
bitsPerFrame = (uint8_t)(((EXAMPLE_DSPI_MASTER_BASEADDR->CTAR[commandStruct.whichCtar] & SPI_CTAR_FMSZ_MASK) >> SPI_CTAR_FMSZ_SHIFT) + 1U);
tmpMCR = EXAMPLE_DSPI_MASTER_BASEADDR->MCR;
if ((0U != (tmpMCR & SPI_MCR_DIS_RXF_MASK)) || (0U != (tmpMCR & SPI_MCR_DIS_TXF_MASK)))
{
fifoSize = 1U;
}
else
{
fifoSize = FSL_FEATURE_DSPI_FIFO_SIZEn(EXAMPLE_DSPI_MASTER_BASEADDR);
}
fifoSize=1U;

data Reading Part

スポイラ

while (1)
{
rxData1=0;
GPIO_PortClear(GPIOC, 1U << 4U); //PTC4 Convst
GPIO_PortSet(GPIOC, 1U << 4U); //PTC4 Convst
while(GPIO_PinRead(GPIOC, 12U) == true){;
//wait for conversions to be completed
}
DSPI_ClearStatusFlags(EXAMPLE_DSPI_MASTER_BASEADDR, (uint32_t)kDSPI_AllStatusFlag);
DSPI_ClearStatusFlags(EXAMPLE_DSPI_SLAVE_BASEADDR, (uint32_t)kDSPI_AllStatusFlag);

//txData = masterXfer.txData;
//rxData = masterXfer.rxData;
remainingSendByteCount = masterXfer.dataSize;
remainingReceiveByteCount = masterXfer.dataSize;

EXAMPLE_DSPI_MASTER_BASEADDR->MCR &= ~SPI_MCR_HALT_MASK;
EXAMPLE_DSPI_SLAVE_BASEADDR->MCR &= ~SPI_MCR_HALT_MASK;

while (remainingSendByteCount > 0U)
{
if (remainingSendByteCount <= 2U)
{
wordToSend = dummyData;

EXAMPLE_DSPI_MASTER_BASEADDR->PUSHR = lastCommand | wordToSend; //Master send Dummy DATA
// EXAMPLE_DSPI_SLAVE_BASEADDR->PUSHR = lastCommand | wordToSend; //Slave send Dummy DATA

EXAMPLE_DSPI_MASTER_BASEADDR->SR = (uint32_t)kDSPI_TxFifoFillRequestFlag; /*!< The status flags are cleared by writing 1 (w1c).*/
EXAMPLE_DSPI_SLAVE_BASEADDR->SR = (uint32_t)kDSPI_TxFifoFillRequestFlag; /*!< The status flags are cleared by writing 1 (w1c).*/

remainingSendByteCount -= 2U;

while (remainingReceiveByteCount > 0U)
{
if ((uint32_t)kDSPI_RxFifoDrainRequestFlag ==
(EXAMPLE_DSPI_MASTER_BASEADDR->SR & (uint32_t)kDSPI_RxFifoDrainRequestFlag))
{
masterRxData[rxData1] = (uint16_t)EXAMPLE_DSPI_MASTER_BASEADDR->POPR; //read Master
EXAMPLE_DSPI_MASTER_BASEADDR->SR = (uint32_t)kDSPI_RxFifoDrainRequestFlag;

slaveRxData[rxData1] = (uint16_t)EXAMPLE_DSPI_SLAVE_BASEADDR->POPR; //read slave
EXAMPLE_DSPI_SLAVE_BASEADDR->SR = (uint32_t)kDSPI_RxFifoDrainRequestFlag;

++rxData1;

remainingReceiveByteCount -= 2U;

}

}
}
else
{
wordToSend = dummyData;

EXAMPLE_DSPI_MASTER_BASEADDR->PUSHR = command | wordToSend;
EXAMPLE_DSPI_SLAVE_BASEADDR->PUSHR = command | wordToSend;
remainingSendByteCount -= 2U;

EXAMPLE_DSPI_MASTER_BASEADDR->SR = (uint32_t)kDSPI_TxFifoFillRequestFlag;
EXAMPLE_DSPI_SLAVE_BASEADDR->SR = (uint32_t)kDSPI_TxFifoFillRequestFlag;

while (((remainingReceiveByteCount - remainingSendByteCount) / 2U) >= fifoSize)
{
if ((uint32_t)kDSPI_RxFifoDrainRequestFlag ==
(EXAMPLE_DSPI_MASTER_BASEADDR->SR & (uint32_t)kDSPI_RxFifoDrainRequestFlag))
{
masterRxData[rxData1] = (uint16_t)EXAMPLE_DSPI_MASTER_BASEADDR->POPR; //read Master
EXAMPLE_DSPI_MASTER_BASEADDR->SR = (uint32_t)kDSPI_RxFifoDrainRequestFlag;

slaveRxData[rxData1] = (uint16_t)EXAMPLE_DSPI_SLAVE_BASEADDR->POPR; //read Slave
EXAMPLE_DSPI_SLAVE_BASEADDR->SR = (uint32_t)kDSPI_RxFifoDrainRequestFlag;

++rxData1;
remainingReceiveByteCount -= 2U;

}
}
}
}

int ii=0;
for (int k = 0; k < 8; k++) {
// highByte = masterRxData[ii+1];
// lowByte = masterRxData[ii];
// ii=ii+2;
datavoltages[k] = ((int16_t)(masterRxData[k]))*qq;
datavoltages[k+4] = ((int16_t)(slaveRxData[k]))*qq;
}

}
}

0 件の賞賛
返信
1 解決策
4,489件の閲覧回数
GRK
Contributor I

Thanks for your reply. Actually i was able to solve the problem. the code was working fine. i was able to get 104ksps. 

i didn't connected the MOSI (FRDM) > SDI (ad7606b). after connecting them the slave was able to read the data as well. i am not using the MOSI as i am using hardware mode so i didn't connected it before. below are some captures.

spi.PNGspi.PNG

below is the spi sampling speed capture

spi2.PNGspi2.PNG

 

i have two more questions.

1) Is there a way to increase the sampling speed?

2) the 16bit data i received is right shifted for all 8 channels.

      ie  instead of     0010 1010 0011 1011

     i am getting        0001 0101 0001 1101

 

Regards.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,442件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @GRK ,

1) The sampling of the slave is according to the bus clock and should be able to sample the signal without problems.

2) Can you try connecting the master interface to the slave interface to check if the problem is the sampling rate or something with the ADC?

Best Regards,

Alexis Andalon

0 件の賞賛
返信
4,498件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @GRK ,

Is possible to share some captures of the SPI lines?

Best Regards,

Alexis Andalon

0 件の賞賛
返信
4,490件の閲覧回数
GRK
Contributor I

Thanks for your reply. Actually i was able to solve the problem. the code was working fine. i was able to get 104ksps. 

i didn't connected the MOSI (FRDM) > SDI (ad7606b). after connecting them the slave was able to read the data as well. i am not using the MOSI as i am using hardware mode so i didn't connected it before. below are some captures.

spi.PNGspi.PNG

below is the spi sampling speed capture

spi2.PNGspi2.PNG

 

i have two more questions.

1) Is there a way to increase the sampling speed?

2) the 16bit data i received is right shifted for all 8 channels.

      ie  instead of     0010 1010 0011 1011

     i am getting        0001 0101 0001 1101

 

Regards.

0 件の賞賛
返信