FRDM-K64 break in IRQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64 break in IRQ

ソリューションへジャンプ
1,778件の閲覧回数
oaf
Contributor IV

I've got into a serious problem today when trying to set a breakpoint in an IRQ function on my FRDM-K64 board.

When the breakpoint is hit the console is continuously showing some read from target, it will not stop

and the stack-frame is only partly filled in namely the function-name of the break-point function

is shown but not the previous ones....

The HDTR Debug [GDB SEGGER J-Link Debugging] JLinkGDBServerCL:

Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)

Read 2 bytes @ address 0x00000584 (Data = 0xB408)

Read 2 bytes @ address 0x00000586 (Data = 0xB662)

Read 2 bytes @ address 0x00000588 (Data = 0x4790)

Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)

Read 2 bytes @ address 0x00000584 (Data = 0xB408)

Read 2 bytes @ address 0x00000586 (Data = 0xB662)

Read 2 bytes @ address 0x00000588 (Data = 0x4790)

Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)

Read 2 bytes @ address 0x00000584 (Data = 0xB408)

Read 2 bytes @ address 0x00000586 (Data = 0xB662)

Read 2 bytes @ address 0x00000588 (Data = 0x4790)

Read 4 bytes @ address 0x0000058A (Data = 0xBC08B672)

タグ(3)
0 件の賞賛
返信
1 解決策
1,643件の閲覧回数
oaf
Contributor IV

It seems that the problem is that GDB is trying to get an infinite stack-backtrace.

The solution is to add this command to the Debugger->Commands:

    set backtrace limit 20

Ref:

KDS debug for K22F120M in interrupt enviroment.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,644件の閲覧回数
oaf
Contributor IV

It seems that the problem is that GDB is trying to get an infinite stack-backtrace.

The solution is to add this command to the Debugger->Commands:

    set backtrace limit 20

Ref:

KDS debug for K22F120M in interrupt enviroment.

0 件の賞賛
返信