FRDM 16Kez - RTE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM 16Kez - RTE

1,259件の閲覧回数
Andrei13
Contributor III

I made a new project based on FRDM 16KEZ SDK, and i included drivers from peripherals and config the pins and clocks. How i generate the RTE_Device.h? I see it suppose to be in board folder, but there are files generated from the pins, peripherals tools. Ty!

0 件の賞賛
返信
1 返信

1,237件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Seems that you are refer to the frdmke16z_cmsis_lpi2c_int_b2b_transfer_master example. Please add LPI2C CMSIS Driver when you create new project.

lpi2c_cmsis LPI2C CMSIS Driver RTE_Device.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信