FNET license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FNET license

2,546件の閲覧回数
thesz
Contributor I

Can I use the FNET TCP/IP Stack library in my commercial product without being required to allow everyone to rebuild the firmware? Am I required to publish the object code of my code to allow a rebuild?

Because I don't understand the meaning/purpose of the 'linking exception'...

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,371件の閲覧回数
perlam_i_au
Senior Contributor I

As you can see in the GNU LGPL 3v licensing will be affected depending on how interrelated are the library and the application (as it is defined on the GNU LESSER GENERAL PUBLIC LICENSE definitions.

In this case I suggest you to enter a Service Request in order to determine if your application licensing is affected or not depending on the usage of FNET.

0 件の賞賛
返信

2,371件の閲覧回数
thesz
Contributor I

My firmware is one big binary for the K60 controller. I don't have modules / dll's oder .a files which the user can replace. My code and the FNET code are combined into one binary.

I already tried to understand 'LGPL': I have to publish my .o files to allow everyone to rebuild my firmware with the latest FNET source code

I don't understand 'linking exception': What does this mean?

Do I have to publish my .o files if I use FNET?

0 件の賞賛
返信

2,371件の閲覧回数
perlam_i_au
Senior Contributor I

Freescale cannot provide legal advertisement, in this case licensing, I suggest you to consult this topic with your lawyer.

0 件の賞賛
返信