FNET TCP/IP stack demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FNET TCP/IP stack demo

ソリューションへジャンプ
3,136件の閲覧回数
ec0359
Contributor II

     Hello,

I would like to try the FNET TCP/IP stack demo, how can we open one the four projects (benchmark, boot, shell, shell_boot) with Codewarrior 10.2.

     Thank you for your help.

ラベル(1)
タグ(1)
1 解決策
2,776件の閲覧回数
butok
NXP Employee
NXP Employee

Hi,

The simplest way is just drag and drop a .project file to your workspace.

(For example Kirin3 shell demo cw10.2 project file is in: fnet\fnet_demos\mcf52259\shell\cw10.2\m52259evb_shell\.project)

Best regards,

Andrey

元の投稿で解決策を見る

2 返答(返信)
2,777件の閲覧回数
butok
NXP Employee
NXP Employee

Hi,

The simplest way is just drag and drop a .project file to your workspace.

(For example Kirin3 shell demo cw10.2 project file is in: fnet\fnet_demos\mcf52259\shell\cw10.2\m52259evb_shell\.project)

Best regards,

Andrey

2,776件の閲覧回数
ec0359
Contributor II

Thank you Andrey, it works very good, now i have to modify this demo to make my application.

  Elio

0 件の賞賛
返信