FLEXIO Acquisition frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FLEXIO Acquisition frequency

1,079 次查看
lacouturepatric
Contributor I
Hello,

I am using the TWR-K80F150M board, MCUXpresso IDE v10.0.0_344 and SDK_2.2_TWR-K80F150M.
 
For my project, i should acquire 4 serial data at 16 MHz which must be saved into sd card. For the acquisition, I use FLEXIO module and the “API FLEXIO CAMERA Receive in EDMA way” : http://mcuxpresso.nxp.com/apidoc/2.0/group__flexio__camera.html.
With the API, I succeed receiving the 4 data until 1 MHz (counter data generated from an FPGA, FLEXIO + EDMA). the FlexIO was configured to input data with an external clock's drive. I did not succeed more than 1 MHz.
 
Who can increase the frequency, is there any configuration on the flexio ?
 
I think If FlexIO is configured to input data with an external clock's drive, the clock frequency has an upper limit of 1/6 FlexIO clock frequency. For K80, the limit is 25MHz.   
Thank you for your help,
Regards,
Patrice

 

标记 (2)
0 项奖励
回复
0 回复数