FLASHING MK60,MK66

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLASHING MK60,MK66

2,241 Views
durgasivakrishn
Contributor III

Hi,

I complted two projects using MK66FN2M0VLQ18 and MK60DN512VLQ10 now they are in production,

To flash my code I am using KEIL, I want to use some application to flash the devices by selecting the .hex file or .out file, is there any application to flashing the devices.

Looking forward to your reply,

Regards,

B.Durga sivakrishna

0 Kudos
Reply
2 Replies

2,130 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

If you use Jlink to download code, you can download Segger JFlash tools. It is free. If you use P&E Multilink, Pemicro also has a tool. But it is not free. But if you use ulink/CMSIS-DAP, it seems there is no software can use it to download hex file.

Regards,

Jing

2,130 Views
durgasivakrishn
Contributor III

Hi Jing,

Thanks for your replay, I have only ulink2.

Regards,

B.Durga sivakrishna

0 Kudos
Reply