FIT and reliability test report for the two components?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FIT and reliability test report for the two components?

1,751 Views
tmao
Contributor I

Can I request you to share the FIT data and Reliability test report for the following two components: P82B96TD and 74LVC1G06GW. If possible can you also provide any other documents associated with the FIT and reliability such as the total number of samples tested so far, test duration and test temperature details? Finally, can I consider that Ea=0.7eV and CL (Confidence Level) = 60%

Thanks a lot !

0 Kudos
Reply
2 Replies

1,490 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Tony

For the P82B96TD you can find the FIT =2.0 on the following link:

Dual bidirectional bus buffer|NXP

For the 74LVC1G06GW FIT = 3.87

inverter with open-drain output|NXP

for more detail about the parameter for the test, please help me to create a new case on the following link:

Sales and Support|NXP

under

Regards

Vicente Gomez

1,490 Views
karina_valencia
NXP Apps Support
NXP Apps Support

vicentegomez​ can you help  to  review this case?

0 Kudos
Reply