FDRM K66 pin assignment searchable table?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FDRM K66 pin assignment searchable table?

1,639件の閲覧回数
pleary
Contributor I

Is the table in the K-66 reference manual, which begins on page 186, section 11.3.1 K66 Signal Multiplexing and Pin Assignments, available in a searchable/editable format such as .csv or .xls?  I understand how the pin assignments work, but using search function is difficult in the pdf format, and I'd like be able to add additional content. Please share if anyone has this available.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,563件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paul

The uTasker project contains device simulations which include pin mux assignment.
That means that it includes tables (in code) that can also be used as input to spread sheets and such.

I have attached the file kinetis_port_K26_K65_K66.h which has an array table of the assignments which you can probably use.

Regards

Mark

uTasker - for more performance and faster, cheaper product development

0 件の賞賛
返信