FDBM KL46Z and MMA8451Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FDBM KL46Z and MMA8451Q

1,435 Views
frdmcharly
Contributor III


Hello! Someone have a good example of FDBM KL46Z and MMA8451Q?

I am working on this project​ and I have one error writting the I2C registers.

I don't know why the line 216 of this code Kinetis-ARM/Accelerometro_driver.c don't write the register.

0 Kudos
Reply
1 Reply

1,203 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Carlos,

  Actually, in the NXP FRDM web, there has the according MMA8451Q sample code, please download the code from this link:

http://cache.nxp.com/files/32bit/software/KL46_SC.exe?fpsp=1&WT_TYPE=Lab%20and%20Test%20Software&WT_...

After you install it, you can find the code in folder:kinetis_kl46_sc_rev2\klxx-sc-baremetal\build\iar\FRDMKL46_Demo

Wish it helps you!

If you still have question, please contact with me!


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply