Extract SerialNumber File from Cyclone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Extract SerialNumber File from Cyclone

1,204 Views
night
Contributor II

Hi,

I'm using Cyclone Max for burn Kinetis devices, and autogenerate serial numbers with it. I use the file .se created with "Serialize" software tool for generate the first number and the structure. But I have a question:

It is possible to extract this "serial file" from Cyclone Max when I need to put another SAP file in? When I erase the SAP file, I need to regenerate the file with the last serial number using serialize, and put it in the compilation again. It is possible to save it FROM the Cyclone for not regenerate the .ser file with the "Serialize" tool?

Very Thanks.

          Miguel Ángel.

Tags (3)
0 Kudos
Reply
0 Replies