External Clock For KEA-128?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Clock For KEA-128?

1,211件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    I want to know which is the best External Clock Mode For KEA-128 in terms of Accuracy and Reliability?

ラベル(2)
0 件の賞賛
返信
1 返信

1,077件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vignesh,

      The accuracy and Reliability is mainly determined by the clock souce.

      But to the clock mode with the same clock source, I suggest you use the FLL.

    Please read the FLL function:

Frequency-locked loop - Wikipedia, the free encyclopedia

    The clock mode with FLL will more stable than other none FLL mode.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信