External Clock For KEA-128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

External Clock For KEA-128?

1,271 Views
vigneshbalaji
Senior Contributor I

Hi,

    I want to know which is the best External Clock Mode For KEA-128 in terms of Accuracy and Reliability?

0 Kudos
Reply
1 Reply

1,137 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vignesh,

      The accuracy and Reliability is mainly determined by the clock souce.

      But to the clock mode with the same clock source, I suggest you use the FLL.

    Please read the FLL function:

Frequency-locked loop - Wikipedia, the free encyclopedia

    The clock mode with FLL will more stable than other none FLL mode.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply