Execution speed in VLPR Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Execution speed in VLPR Mode

1,276 Views
shrejjjhh
Contributor III

Hi,

I am using MKL15Z128CAD4R. I have configured the controller to VLPR mode at 2MHz SystemCoreClock. But this increases the execution time and hence my application gets slower. Is there any way to increase the instruction execution speed? 

Regards,

Shrey

0 Kudos
Reply
1 Reply

1,214 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Shrey,

In the reference manual you will find the following information in the table 5-1. 

pastedImage_2.png

You can increase the speed of the clock up to 4MHz. If you want to increase more the execution speed of the instructions then you will need to exit VLPR mode so you can speed the clock up to 48MHz. 

Link to the reference manual

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply