Execution speed in VLPR Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Execution speed in VLPR Mode

1,311件の閲覧回数
shrejjjhh
Contributor III

Hi,

I am using MKL15Z128CAD4R. I have configured the controller to VLPR mode at 2MHz SystemCoreClock. But this increases the execution time and hence my application gets slower. Is there any way to increase the instruction execution speed? 

Regards,

Shrey

0 件の賞賛
返信
1 返信

1,249件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Shrey,

In the reference manual you will find the following information in the table 5-1. 

pastedImage_2.png

You can increase the speed of the clock up to 4MHz. If you want to increase more the execution speed of the instructions then you will need to exit VLPR mode so you can speed the clock up to 48MHz. 

Link to the reference manual

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信