Execution Failure in flash loader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Execution Failure in flash loader

3,054件の閲覧回数
bharthyalla
Contributor I

Hello Guys,

 

I am Using MKM34Z128ACLL5 and IAR Workbench version 7.20 while debugging I am Getting this Error  EXECUTION FAILURE IN FLASH LOADER.what is the reason for this error and its cause.

0 件の賞賛
返信
1 返信

2,296件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Bharth Yalla

What debug interface are you using? This problem normally is related with the reset pin of your debugger, so please check this pin in your device. Also you could try to check your reset option in Project->Options->Debugger->(your debugger interface) and try to select the option that you need. For example for jlink.

pastedImage_4.png

Hope this could helps.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信