Execution Failure in flash loader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Execution Failure in flash loader

3,095 Views
bharthyalla
Contributor I

Hello Guys,

 

I am Using MKM34Z128ACLL5 and IAR Workbench version 7.20 while debugging I am Getting this Error  EXECUTION FAILURE IN FLASH LOADER.what is the reason for this error and its cause.

0 Kudos
Reply
1 Reply

2,337 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Bharth Yalla

What debug interface are you using? This problem normally is related with the reset pin of your debugger, so please check this pin in your device. Also you could try to check your reset option in Project->Options->Debugger->(your debugger interface) and try to select the option that you need. For example for jlink.

pastedImage_4.png

Hope this could helps.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply