Execution Failure in flash loader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Execution Failure in flash loader

3,092 次查看
bharthyalla
Contributor I

Hello Guys,

 

I am Using MKM34Z128ACLL5 and IAR Workbench version 7.20 while debugging I am Getting this Error  EXECUTION FAILURE IN FLASH LOADER.what is the reason for this error and its cause.

0 项奖励
回复
1 回复

2,334 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Bharth Yalla

What debug interface are you using? This problem normally is related with the reset pin of your debugger, so please check this pin in your device. Also you could try to check your reset option in Project->Options->Debugger->(your debugger interface) and try to select the option that you need. For example for jlink.

pastedImage_4.png

Hope this could helps.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复