Execute command not jumping to LED blink application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Execute command not jumping to LED blink application

2,226 Views
arunkannan
Contributor III

We have the LED blink application at 0x9000 and when we run execute command in blhost as below it is not going to application and LED is not blinking. 

C:\blhost\win>blhost.exe -p COM4,115200 execute 0x9000 0 0x20002f80
Ping responded in 1 attempt(s)
Inject command 'execute'
Successful generic response to command 'execute'
Response status = 0 (0x0) Success.

Kindly let me know how to make it jump to 0x9000 to make LED blink

Labels (1)
0 Kudos
Reply
3 Replies

2,153 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport
Hello, could you elaborate further on your issue? is not enough to analyze your behavior. What kind of IDE are you using and what is your target MCU? Are you using an EVK or custom board?
Is this HardFualt happening on an example SDK? Could you share the name of the project or the project to replay the issue and the steps?
 
Best regards,
Pavel
0 Kudos
Reply

2,194 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, but I´m following your 3 cases, I will continue this in the internal where you upload some images.

Best regards,
Pavel

0 Kudos
Reply

2,186 Views
arunkannan
Contributor III

You can close other cases. Resolved those issues. Need help on this one alone.

0 Kudos
Reply