Example for TWR-K40D100M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example for TWR-K40D100M

2,120 Views
ilias
Contributor I

Hello.

I am looking for any example that could work with the board TWR-K40D100M with MK40DX256VMD10 CPU.

In SDK 1.3, there is no such an example. The examples for TWR-K60D100M seem to be not compatible with the specific board (e.g: gpio_demo, hello_world, etc).

Is there anybody that is using this board and  could help me to set it up? Any example would saved be a lot of time.

Thanks in advance.

There are 10 types of people. Those who understand the binary system of numbers and those who don't.
Labels (1)
Tags (1)
2 Replies

1,994 Views
dsamarin
Contributor I

Same here. Is there KDS 1.3 or 2.0 example code for the K40's Tower platform?

0 Kudos
Reply

1,994 Views
mjbcswitzerland
Specialist V

Hi Daniel

I understand that the K40 (being quite an old chip) will not be supported in the newer NXP environments. I suspect this to be due to the fact that the existing framework is too "high-maintenance" (and costly) to allow non-targeted processors to be continuously supported as new types are added.

However you can get all support for professional requirements at:
http://www.utasker.com/kinetis/TWR-K40D100M.html
including KDS, CW, etc.

Regards

Mark

0 Kudos
Reply