Example KV44F256 for usage of eFlexPWM with 312ps resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example KV44F256 for usage of eFlexPWM with 312ps resolution

3,044件の閲覧回数
katha
Contributor II

Hello,

I am looking for example code to use the eFlexPWM with 312ps resolution  within a KV44F256. Examples I found in SDK only provide setting the dutycyle 0...100%.

Thanks and regards

ラベル(1)
4 返答(返信)

2,684件の閲覧回数
katha
Contributor II

Hi XiangJun,

that is what my question was for: could you send me the clocks configuration within a *.mex file?

Thank you and regards

Katharina

2,684件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Katharina,

Pls refer to the documentation, which describes the nano-edge placement feature of the KV46.

https://community.nxp.com/docs/DOC-341621

Hope it can help you

BR

XiangJun Rong

2,684件の閲覧回数
katha
Contributor II

Hi XiangJun,

could you please send the .mex file including the clocks configuration

Thanks

Katharina

2,684件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Katharina,

I think the project does not use *.mex file, regarding the clock configuration, the clock configuration tools is not used, the clock configuration code for example PLL is integrated in the code in the main.c

BR

XiangJun Rong