Ethernet for K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet for K60

2,330件の閲覧回数
josemartinez
Contributor III

Hi everyone,

I'm new with Kinetis, I want to use Ethernet with K60 but I don't want to use MQX for it, is there any stack to use Ethernet without using MQX?

In case it has, where could I find it?

I'm new with it and it will be very apreciated any help

Thanks in advance.

Jose

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,063件の閲覧回数
josemartinez
Contributor III

Hello,

I have been looking at FNET and I show that I can use MK60N512 and MK70FN1M. When I want to create a new project in CW 10.4 I can't find MK60N512 but MK70FN1M is on the list of CW.

On the list that CW has, it's  MK60DN512 and PK60N512, something of those is compatible with MK60N512 that FNET have in its list? I would like to use MK60DN512 if possible.

Thanks

Jose

0 件の賞賛
返信

2,063件の閲覧回数
albertovargas
NXP Employee
NXP Employee

Try using the stack for MK60DN512. K60 and K70 are quite different, so if you're using a K60, stay with the stack for K60.

0 件の賞賛
返信

2,063件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Have a look at FNET:

http://fnet.sourceforge.net/

(or google for "FNET Freescale")

2,063件の閲覧回数
josemartinez
Contributor III

I'm going to have a look.

Thanks

0 件の賞賛
返信