Ethernet for K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet for K60

2,328 Views
josemartinez
Contributor III

Hi everyone,

I'm new with Kinetis, I want to use Ethernet with K60 but I don't want to use MQX for it, is there any stack to use Ethernet without using MQX?

In case it has, where could I find it?

I'm new with it and it will be very apreciated any help

Thanks in advance.

Jose

Labels (1)
0 Kudos
Reply
4 Replies

2,061 Views
josemartinez
Contributor III

Hello,

I have been looking at FNET and I show that I can use MK60N512 and MK70FN1M. When I want to create a new project in CW 10.4 I can't find MK60N512 but MK70FN1M is on the list of CW.

On the list that CW has, it's  MK60DN512 and PK60N512, something of those is compatible with MK60N512 that FNET have in its list? I would like to use MK60DN512 if possible.

Thanks

Jose

0 Kudos
Reply

2,061 Views
albertovargas
NXP Employee
NXP Employee

Try using the stack for MK60DN512. K60 and K70 are quite different, so if you're using a K60, stay with the stack for K60.

0 Kudos
Reply

2,061 Views
BlackNight
NXP Employee
NXP Employee

Have a look at FNET:

http://fnet.sourceforge.net/

(or google for "FNET Freescale")

2,061 Views
josemartinez
Contributor III

I'm going to have a look.

Thanks

0 Kudos
Reply