Ethernet controller & SD at about 30cm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet controller & SD at about 30cm

1,350 Views
Microfelix
Contributor IV

 

hello

I'm doing a project where I use the ethernet and the SD with the K60.
I was wondering if you can place both the Ethernet controller that SD at about 30cm from the microcontroller via a flat cable.

There are no contraindications and has already been tested?

thanks

 

Maurizio

0 Kudos
Reply
1 Reply

1,191 Views
B_Sandor
Contributor I

Maurizio!

Could you help me to design an ethernet connect for K60?

I didn't find example how do I connect  K60 to RJ45.

Could you send me a schematic for it? ([email protected])

Thx.

0 Kudos
Reply