Ethernet Module Clock on MKV58F1M0VLQ24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Module Clock on MKV58F1M0VLQ24

ソリューションへジャンプ
1,830件の閲覧回数
SMNJS
Contributor II

Hello,

In the reference manual of the KV5XP144M240RM (MKV58F1M0VLQ24 µC in my case) it is stated in table 6-1. Module clocks in chapter 6.5 Module clocks, that the ethernet module uses:

  • System (CPU) clock
  • Bus/Flash clock

as Bus interface clock.
As I already observed, that the systemclock e.g. is affecting the MDC for the PHY interface, I now wonder what is the correlation between the Ethernet Module and the Bus/Flash clock?

How does this clock affect the Ethernet Module?
I didn't find any information about this correlation besides the mentioned table in the reference manual.

Kind regards,

Julian

タグ(2)
0 件の賞賛
返信
1 解決策
1,822件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,823件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

0 件の賞賛
返信