Ethernet Module Clock on MKV58F1M0VLQ24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Module Clock on MKV58F1M0VLQ24

Jump to solution
1,820 Views
SMNJS
Contributor II

Hello,

In the reference manual of the KV5XP144M240RM (MKV58F1M0VLQ24 µC in my case) it is stated in table 6-1. Module clocks in chapter 6.5 Module clocks, that the ethernet module uses:

  • System (CPU) clock
  • Bus/Flash clock

as Bus interface clock.
As I already observed, that the systemclock e.g. is affecting the MDC for the PHY interface, I now wonder what is the correlation between the Ethernet Module and the Bus/Flash clock?

How does this clock affect the Ethernet Module?
I didn't find any information about this correlation besides the mentioned table in the reference manual.

Kind regards,

Julian

0 Kudos
Reply
1 Solution
1,812 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
1,813 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

0 Kudos
Reply