Ethernet Module Clock on MKV58F1M0VLQ24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet Module Clock on MKV58F1M0VLQ24

跳至解决方案
1,833 次查看
SMNJS
Contributor II

Hello,

In the reference manual of the KV5XP144M240RM (MKV58F1M0VLQ24 µC in my case) it is stated in table 6-1. Module clocks in chapter 6.5 Module clocks, that the ethernet module uses:

  • System (CPU) clock
  • Bus/Flash clock

as Bus interface clock.
As I already observed, that the systemclock e.g. is affecting the MDC for the PHY interface, I now wonder what is the correlation between the Ethernet Module and the Bus/Flash clock?

How does this clock affect the Ethernet Module?
I didn't find any information about this correlation besides the mentioned table in the reference manual.

Kind regards,

Julian

标记 (2)
0 项奖励
回复
1 解答
1,825 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,826 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @SMNJS ,

Here bus/flash clock is used to read/write register in Ethernet module.

 

Regards,

Jing

0 项奖励
回复