Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M

2,196 次查看
muhammad_qasim
Contributor I

Hi

I have successfully run my Ethernet Driver on TWR-SER board for TWR-K70F120M but not working on TWR-SER2.

1. Is Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M?  According to this link, (Line: 241) it is not supported?

2. If supported, then is there any change in signal settings like (MDC, MDIO, CRS_DV, RXDn, RXErr, TXDn, TXEN and RMII_REF_CLK) as compared to TWR-SER board?

Regards

标记 (2)
0 项奖励
回复
4 回复数

1,874 次查看
perlam_i_au
Senior Contributor I

TWR-SER2 has dual RMII and also signle MII port (this is not part of the TWR-SER features), and just as Mark mentioned before there are certainly changes between both boards it means that you probably need to make some changes on the pins.

I suggest you to take a look and compare TWR-SER_Schematic VS TER-SER2_Schematic, below you will find a list of pins that have changed from SER to SER2 (is referenced on the J15A and J15B elevator connector of SER2 board), I hope you find it useful.

J15A

PinRelated Change
B12-B15, B17-B20RMII & MII
B55,B57,B59,B61,B65IRQ (missing connection in reference to TWR-SER)
A57USB (missing connection in reference to TWR-SER)
A43-A44ELE RX/TX (from SER) changed to UART RX/TX
A35GPIO6 (from SER) changed to USB_VBUS
A7-A8SDA0 and SCI0 signals has been removed (in reference to SER)
A9ELE_CTC has been removed (in reference to SER)

J15B

PinRelated Change
D1,C1Has been connected to 5v power supply
D3,D82,C82,C36,C3,C4Has been connected to 3.3v power supply
D13,D15,D19-D25,C16,C19-C20RMII has been connected to these pins
C21-C25,C10-C11ULPI has been connected to these pins
C41-C48UART has been connected to these pins


Have a nic day :P,
Perla

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,874 次查看
muhammad_qasim
Contributor I

Hi

Ethernet is working on TWR-SER2 but there is a packet loss against PING Command (after random time). Did following pin muxing

PORTA_PCR12-17 = 0x00000400;

PORTB_PCR0 = 0x00000400 | PORT_PCR_ODE_MASK | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;

PORTB_PCR1 = 0x00000400;

And only enabled this clock

sim->SCGC2 |= SIM_SCGC2_ENET_MASK;

And there was no jumper on J8 and J9. Switch settings was 11000000 and 10100000

0 项奖励
回复

1,874 次查看
perlam_i_au
Senior Contributor I

I have been looking for information but I am pretty sure that if your project works fine until you send PING command something weird should be happening, could you please share your project? I would like to reproduce the error.

0 项奖励
回复

1,874 次查看
mjbcswitzerland
Specialist V

Hi

The TWR-K70F120M can be used with "one" of the TWR-SER2 RMII connections. There are no connection difference so the same code can be used for configuring the required peripheral lines as used with TWR-SER board.

The PHY is of course different and there is no PHY interrupt available so it may be necessary to poll the PHY to get link state information.

Check also jumper settings on the TWR-SER2 according to the details in its user's manual.

Regards

Mark

0 项奖励
回复